Configure Analyzer

Use the triple bar icon on the top left of the display to access the Configure Analyzer selection. The Configure Analyzer screen is used for performing generation-to-analysis workflow. The "Auto Configure Analyzer" button will automatically transfer the setup from the Source to a Keysight X-Series Signal Analyzer, in order to measure the desired signal from the Source. If you are generating a 3GPP 5G New Radio, NR-V2X, or Custom IQ signal via the Applications menu of the signal generator, and the corresponding application is licensed on the analyzer, the analyzer will perform demodulation of the signal. Otherwise, the analyzer will auto-tune on the signal being generated. The Keysight X-Series Signal Analyzer requires firmware version x.35.00 or greater for the demodulation to be performed.

GUI Location

System Menu (triple bar icon) > Configure Analyzer

Remote Instrument

Use Device List

Specify Device for Auto Configure Analyzer

Connection Type

Test Connection

Output Channel

VISA Address of Receiver

Source Block

Auto Configure Analyzer

Remote Instrument

The "Click to change connection" box opens the Remote Instrument screen, which provides settings for remotely connecting to the Keysight X-Series signal analyzer. The default values for the signal analyzer are pre-populated. Refer to your signal analyzer if the values are different from the default.

Use Device List

This checkbox enables the Device List to be the sole method of specifying a Spectrum Analyzer to be used for a channel’s Auto Configuration.

A Closedscreen appears, showing the name and type of the current device, if any, and a Configure Device button.

The Configure Device button takes you to the ClosedDevice List Manager screen where you can select and configure other devices.

To configure external devices in the Device List, see Device List.

GUI Location

System Menu (triple bar icon) > Configure Analyzer > Click to change connection > select Use Device List

SCPI Command

[:SOURce][:RF<channel>]:ASANalyzer:DLISt ON|OFF|1|0

[:SOURce][:RF<channel>]:ASANalyzer:DLISt?

SCPI Example

RF3:ASAN:DLIS ON

RF3:ASAN:DLIS?

Preset

This is unaffected by a Preset but is set to OFF on a "Restore System Settings to Default Values."

State Saved

Persistent, survives preset and power cycle but not saved in the instrument state.

Range

ON | OFF | 1 | 0

Specify Device for Auto Configure Analyzer

Specifies a Spectrum Analyzer from the Device List to be used for the specified channel’s Auto Configuration.

To configure external devices in the Device List, see Device List.

GUI Location

System Menu (triple bar icon) > Configure Analyzer > Click to change connection > select Use Device List checkbox > Configure Device > Device List Manager

SCPI Command

[:SOURce][:RF<channel>]:ASANalyzer:DEVice <name>

[:SOURce][:RF<channel>]:ASANalyzer:DEVice?

SCPI Example

RF3:ASAN:DEV "mySpectumAnalyzer"

Notes

If the specified device does not exist in the Device List, the following error will be raised:

-220,"Parameter error; Specified device does not exist"

If the specified device is not a Spectrum Analyzer the following error will be raised:

-220,"Parameter error; Auto Configure Analyzer requires a Spectrum Analyzer device type"

Couplings

If the device currently selected from the Device List is removed, this setting will default to NONE

Value will only be utilized by hardware when Use Device List for Auto Configure Analyzer is set to ON.

Preset

This is unaffected by a Preset but is set to the empty string on a "Restore System Settings to Default Values."

State Saved

Persistent, survives preset and power cycle but not saved in the instrument state.

Connection Type

Select a LAN or USB physical communication connection to the analyzer.

GUI Location

System Menu (triple bar icon) > Configure Analyzer > Click to change connection > Connection Type

LAN

Set LAN Address

Enter the Hostname or IP Address of the analyzer. the LAN address is saved during Save User Preset, allowing you to use User Preset to easily restore the address after startup.

Set Protocol

The values of the protocol settings are standard values for the Keysight X-Series signal analyzers. Changes to the values persist across power-cycling and are not changed by Preset. Use Restore System Settings to Default to return the values to their defaults. The protocol in use much match the setting in the analyzer’s configuration.

The default protocol is HiSLIP which has the highest throughput of the LAN choices.

USB

After connecting your device to a USB port, select it from the drop-down menu. You can also refresh the list of USB connected devices, if necessary.

Test Connection

Use this immediate action to check the communication connection to the analyzer. If successful, a message briefly appears and the VISA address is displayed below the Closedanalyzer block in the Configure Analyzer screen. If unsuccessful, a message briefly appears and is logged in the message queue.

Output Channel

On instruments with more than one channel, you indicate which channel is directed to the signal analyzer.

GUI Location

System Menu (triple bar icon) > Configure Analyzer > Output

SCPI Command

[:SOURce]:SCONfigure:OUTPut <channel>

[:SOURce]:SCONfigure:OUTPut?

SCPI Example

SCON:OUTP 1

Notes

The maximum selection is based on the configuration of the instrument. Use the query SOUR:RF:COUN? to determine the maximum value for the instrument being controlled.

When Use Device List for Auto Configure Analyzer is set to OFF, Visa Address of Receiver is used to specify a Spectrum Analyzer, see VISA Address of Receiver.

When Use Device List for Auto Configure Analyzer is set to ON, Device for Auto Configure Analyzer is used to specify a Spectrum Analyzer, see Specify Device for Auto Configure Analyzer.

Preset

1

Min

1

State Saved

Yes

VISA Address of Receiver

This configures the full VISA address of the receiver to use for Auto Configure Analyzer when the Device List is not being used for those features.

GUI Location

System Menu (triple bar icon) > Configure Analyzer > Click to change connection > Configure Device by selecting the Connection Type, Hostname or IP Address, and Protocol

SCPI Command

:SYSTem:COMMunicate:REMote:ADDRess <string>

:SYSTem:COMMunicate:REMote:ADDRess?

SCPI Example

SYST:COMM:REM:ADDR TCPIP0::10.0.0.1::hislip0::INSTR"

Couplings

Value will only be utilized for Auto Configure Analyzer by hardware when Use Device List for Auto Configure Analyzer is set to OFF.

Preset

This is unaffected by a Preset but is set to an empty string on a "Restore System Settings to Default Values".

State Saved

Persistent, survives preset and power cycle but not saved in the instrument state.

Source Block

The diagram for the signal generator lists the configuration of the Signal and Frequency for each channel. Selecting the source diagram returns to the generator’s main screen.

Auto Configure Analyzer

Select the Auto Configure Analyzer control to send the signal generator’s settings to the signal analyzer.

Using the Configure Analyzer Interface

System Menu

Device List